AXIS#.SAFEPARAM.SLA.FUNCTIONACTIVATION

Description

Indicates whether the Safely Limited Acceleration (SLA) safety functions can be activated. One of the following values is used:

Value Description

0

Never active

1

Ready for activation

2

Always activated

This function can only be used when a safe encoder is configured in the safety parameters.

 

Parameters Editor with Function Activation values shown and circled

Context

For complete SLA information refer to SLA (Safely Limited Acceleration).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1 , 2

Default Value

0 (Never active)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLA.FUNCTIONACTIVATION

3165h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLA.FUNCTIONACTIVATION

3265h

01h

Unsigned8

-

-

Read/Write

No